AnsweredAssumed Answered

bootng zynq zc702+fmcomms5

Question asked by swaxman on Nov 15, 2014
Latest reply on Nov 17, 2014 by brandonj

Hi ,

 

I erased my SD card and loaded the unzipped image in the Zynq quick start page using the win32diskimager application.

I then followed the rest of the instructions, including the boot & tools update scripts.

The SD card seems to be fully occupied with the libraries and projects.

When booting (ZC702+FMCOMMS5) I get the error message below at the end of the boot, and the HDMI screen does not seem to be responding.

 

please help.

 

thanks,

-shai

 

...

 

TCP: cubic registered

NET: Registered protocol family 17

zynq_pm_remap_ocm: OCM pool is not available

zynq_pm_suspend_init: Unable to map OCM.

Registering SWP/SWPB emulation handler

axi-hdmi 70e00000.axi_hdmi: No connectors reported connected with modes

[drm] Cannot find any crtc or sizes - going 1024x768

Console: switching to colour frame buffer device 128x48

axi-hdmi 70e00000.axi_hdmi: fb0:  frame buffer device

axi-hdmi 70e00000.axi_hdmi: registered panic notifier

[drm] Initialized axi_hdmi_drm 1.0.0 20120930 on minor 0

cf_axi_adc 79020000.cf-ad9361-A: ADI AIM (8.00.a) at 0x79020000 mapped to 0xf0078000, probed ADC AD9361-2 as MASTER

random: nonblocking pool is initialized

cf_axi_adc 79040000.cf-ad9361-B: ADI AIM (8.00.a) at 0x79040000 mapped to 0xf0130000, probed ADC AD9361 as SLAVE

rtc-pcf8563 5-0051: low voltage detected, date/time is not reliable.

rtc-pcf8563 5-0051: setting system clock to 2063-07-30 02:54:07 UTC (2952989647)

ALSA device list:

  #0: HDMI monitor

EXT4-fs (mmcblk0p2): warning: mounting fs with errors, running e2fsck is recommended

EXT4-fs (mmcblk0p2): recovery complete

EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)

VFS: Mounted root (ext4 filesystem) on device 179:2.

Freeing unused kernel memory: 196K (c05a0000 - c05d1000)

EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:756: group 18,¢Â¢±ÕÍ?ÉÍEXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:756: group 20, 558 clusters in bitmap, 556 in gd; block bitmap corrupt.

EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:756: group 21, 26423 clusters in bitmap, 26452 in gd; block bitmap corrupt.

EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:756: group 22, 20270 clusters in bitmap, 20211 in gd; block bitmap corrupt.

 

Last login: Thu Jan  1 00:00:09 UTC 1970 on tty1
Welcome to Linaro 12.11 (GNU/Linux 3.15.0-g8da3e74 armv7l)

* Documentation:  https://wiki.linaro.org/

root@linaro-ubuntu-desktop:~# EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:756: group 5, 15995 clusters in bitmap, 16011 in gd; block bitmap corrupt.

Outcomes