AnsweredAssumed Answered

ADV7511W 8-bit 422 SDR max input clock

Question asked by benwang on Nov 14, 2014
Latest reply on Nov 28, 2014 by GuenterL


Hello,

 

I'd like to confirm what is max input clock if ADV7511W is configured as 8-bit 422 SDR model pixel input, as datasheet, the input clock is up to 165MHz on CLK pin, but as "video input connections" table (as attached), if in 8-bit 422 SDR model, the max clock is only 82.5MHz, that means ADV7511 can run only 82.5MHz clock once in 8-bit 422 SDR input mode? would you pls help on this quesiton.

 

Thank you

Attachments

Outcomes