AnsweredAssumed Answered

ADV7611 ; how to transfer 720x480p60 using bt.656 ??

Question asked by luisfynn on Nov 13, 2014
Latest reply on Nov 14, 2014 by mattp

i'am luis in Korea

 

wish you would understand i am poor at ENGLISH.

 

ADV7611 receive 720X480P60 image(RASPBERRY PI)

and i wannt to send 720x480p60 using bt.656 to encoder( not used hs,vs,de)

 

below my code. plz check my code. I2C ADDRESS SETTING is skipped.

 

282 //----------------------------------------------------------------

283      0x98, 0x01, 0x06 ,  // Prim_Mode[3:0] & VFREQ[6:4]

284      0x98, 0x02, 0xF5 ,  // Auto CSC, YCrCb out, Set op_656 bit

285      0x98, 0x03, 0x42 ,  // 36 bit SDR 444 Mode 0

286      0x98, 0x04, 0x60 ,  // OP_CH_SEL & XTAL_FREQ_SEL

287      0x98, 0x05, 0x28 ,  // AV Codes OFF

288      0x98, 0x0B, 0x44 ,  // Power up part

289      0x98, 0x0C, 0x42 ,  // Power up part

290      0x98, 0x14, 0x7F ,  // Max Drive Strength

291      0x98, 0x15, 0x80 ,  // Disable Tristate of Pins

292      0x98, 0x19, 0x83 ,  // LLC DLL phase -720x480p 54Mhz

293      0x98, 0x33, 0x40 ,  // LLC DLL enable

294

295      0x44, 0xBA, 0x01 ,  // Set HDMI FreeRun

296

297      0x64, 0x40, 0x81 ,  // Disable HDCP 1.1 features

298

299      0x68, 0x9B, 0x03 ,  // ADI recommended setting

 

300 #if 0

301      0x68, 0xC1, 0x01 ,  // ADI recommended setting

302      0x68, 0xC2, 0x01 ,  // ADI recommended setting

303      0x68, 0xC3, 0x01 ,  // ADI recommended setting

304      0x68, 0xC4, 0x01 ,  // ADI recommended setting

305      0x68, 0xC5, 0x01 ,  // ADI recommended setting

306      0x68, 0xC6, 0x01 ,  // ADI recommended setting

307      0x68, 0xC7, 0x01 ,  // ADI recommended setting

308      0x68, 0xC8, 0x01 ,  // ADI recommended setting

309      0x68, 0xC9, 0x01 ,  // ADI recommended setting

310      0x68, 0xCA, 0x01 ,  // ADI recommended setting

311      0x68, 0xCB, 0x01 ,  // ADI recommended setting

312      0x68, 0xCC, 0x01 ,  // ADI recommended setting

313 #endif

 

314      0x68, 0x00, 0x08 ,  // Set HDMI Input Port A (BG_MEAS_PORT_SEL = 001b)

315      0x68, 0x02, 0x03 ,  // Enable Ports A & B in background mode

316

317      0x68, 0x83, 0xFC ,  // Enable clock terminators for port A & B

318      0x68, 0x6F, 0x0C,   // ADI recommended setting

319      0x68, 0x85, 0x1F,   // ADI recommended setting

320      0x68, 0x87, 0x70,   // ADI recommended setting

321      0x68, 0x8D, 0x04,   // LFG Port A

322      0x68, 0x8E, 0x1E,   // HFG Port A

323      0x68, 0x1A, 0x8A,   // unmute audio

324      0x68, 0x57, 0xDA,   // ADI recommended setting

325      0x68, 0x58, 0x01,   // ADI recommended setting

326

327      0x68, 0x75, 0x10,   // DDC drive strength

328      0x68, 0x90, 0x04,   // LFG Port B

329      0x68, 0x91, 0x1E,   // HFG Port B

330

331      0x98, 0x03, 0x00,   // 8-bit SDR ITU-656 mode

332      0x98, 0x19, 0xC3,   // LLC DLL phase (Matt)

333      0x98, 0x04, 0x42,   // OP_CH_SEL

334      0x98, 0x05, 0x2C,   // AV code on

Outcomes