AnsweredAssumed Answered

ad9361-iiostream with network backend running on a linux host

Question asked by elvisjohndowson on Nov 13, 2014
Latest reply on Nov 13, 2014 by elvisjohndowson

Hi,

 

How can I run the libiio/examples/ad9361-iiostream.c example, so that it runs on a linux host (RHEL-6.6 64-bit), and uses a network backend to communicate with a ZC706+AD-FMCOMMS3-EBZ board, via an ethernet connection.

 

I've got the ZC706+AD-FMCOMM3-EBZ setup, and I can run the ad9361-iiostream example on the target board, as outlined in the following discussion thread:

 

AD9361+Zedboard and AD9361_iiostream example

 

I've build libiio on my host but when I try to run it, it gives me an error saying:

 

* Acquiring IIO context

ERROR: Unable to create context: No such file or directory

ad9361-iiostream: ad9361-iiostream.c:194: main: Assertion `(ctx = iio_create_default_context()) && "No context"' failed.

 

Regards,

 

Elvis Dowson

Outcomes