AnsweredAssumed Answered

ADV7619 color space conversion

Question asked by tips on Nov 12, 2014
Latest reply on Nov 20, 2014 by GuenterL

Hi,

I'm trying to use the ADV7619 to convert a YCbCr input to RGB output when the source is DVI putting out YCbCr.  I know this signal is out of spec (DVI is RGB only), but I want to be able to handle it anyway.  On the ADV7619/ADV7511 eval board I'm using several registers to do this with the CP block in automatic mode, since I don't want to manually load the coefficients unless I have to.  The registers/bits that seemingly should handle this only cause the pink video to change to various shades of pink.  Does the chip support this conversion?  Specifically, I'm setting

 

CP 69: 14     (enable the CSC)

CP 68: F0     (CSC automatic mode)

CP BD: 08    (use the DPP block)

IO 02: 32      (YCbCr 709 in, rgb out)


Except for this conversion, I'm not using the CP block. 

Any help would be appreciated.


Thanks,

Tim

Outcomes