AnsweredAssumed Answered

Zedboard+AD-FMCOMMS2-EVB, Vivado 2013.4

Question asked by ADI_Wei on Nov 11, 2014
Latest reply on Nov 17, 2014 by AdrianC
Branched to a new discussion

I want to run the no-os code in Vivado 2013.4 with Zedboard, I download the reference design hdl_2014_r1 .

I building the project by running below script. Please help to check whether the script is necessary and complete.

 

cd c:/github/library/util_i2c_mixer

source ./util_i2c_mixer_ip.tcl


cd c:/github/library/axi_clkgen

source ./axi_clkgen_ip.tcl


cd c:/github/library/axi_hdmi_tx

source ./axi_hdmi_tx_ip.tcl


cd c:/github/library/axi_spdif_tx

source ./axi_spdif_tx_ip.tcl


cd c:/github/library/axi_i2s_adi

source ./axi_i2s_adi_ip.tcl


cd c:/github/library/axi_ad9361

source ./axi_ad9361_ip.tcl


cd c:/github/library/axi_dmac

source ./axi_dmac_ip.tcl


cd c:/github/library/util_adc_pack

source ./util_adc_pack_ip.tcl


cd c:/github/library/util_dac_unpack

source ./util_dac_unpack_ip.tcl

 

cd c:/github/projects/fmcomms2/zed

source ./system_project.tcl


There are some errors and warnings showed in the message window in the Vivado. Please check the attachment. Could you please help to give some suggestion to get rid of the errors?

Attachments

Outcomes