AnsweredAssumed Answered

ADXL326 Specification Questions - Clarified

Question asked by danngai on Nov 6, 2014
Latest reply on Oct 19, 2015 by NevadaMark


These questions were submitted previously, but there was a mixup in the part numbers and subsequently the answers were directed using different part.  Anyway, this is for the ADXL326.

 

·         1.  What is the Maximum Measurement Range MAX for ADXL326?  [Show blank in datasheet.]

 

     2.  How is accuracy affected at G levels greater than +/-19G? 

           [Expected output range is 2.583V[+19G] and 0.417V [-19G] at these levels]

 

     3.  Our design can see as acceleration rate as high as 50G in 1 channel and +/-25G in both channels for up to 5

          seconds.  Can the device handle this?   Will the device be damaged in any way?

 

Thank you in Advance!

 

Dan

Outcomes