AnsweredAssumed Answered

FMCOMMS5 iio scope

Question asked by swaxman on Nov 6, 2014
Latest reply on Nov 7, 2014 by larsc

Hi,

 

I am trying to run the iio oscilloscope using the FMCOMMS5+ZC706 boards :

1. I got the binary for the board 1 month ago from you (attached) : when booting, both AD9361 devices are detected, yet at the end of the boot I get the following message:

EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:756: group 22, 20237 clusters in bitmap, 20265 in gd; block bitmap corrupt.

EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:756: group 21, 30523 clusters in bitmap, 30500 in gd; block bitmap corrupt.

Welcome to Linaro 12.11 (GNU/Linux 3.15.0-g73a49b3-dirty armv7l)

* Documentation:  https://wiki.linaro.org/

 

2. I ignored the error above and continued installing iio oscilloscope as instructed on the Linux virtual machine. Once completed I could not find the iioscope icon on the desktop so I ran the OSC executable from within the iio-oscilloscope folder. Once open I could not see any activity on the screen and the device list is empty !

 

PLEASE PROVIDE DETAILED REPLY AND AVOID REFERRING TO WEBPAGES .

 

thanks,

-shai

Outcomes