AnsweredAssumed Answered

AD9364 - Internal ADC

Question asked by aruna_karthi@yahoo.com on Nov 5, 2014
Latest reply on Nov 6, 2014 by tlili

We are using AD9364 in our design, I would like to know if the Internal ADC can be used for converting the RF out put of the Power Amplifier. We are using SKY77764 Power Amplifier. I would like to feed  the Coupled port out put (around 0dBm) of the PA to the ADC and use that value for measuring the Transmit  power of our system. Please let us know if it is feasible. The reason is to avoid one power detector. The frequency of the RF signal would be 700MHz - 2100MHz Range.

Outcomes