AnsweredAssumed Answered

CPLB miss without replacement error

Question asked by VeereshJoladal on Nov 4, 2014
Latest reply on Nov 11, 2014 by Suraj

I am trying to write a program to send data serially over UART in Blackfin-526C. I used the UART driver example available in Cross Core Embedded Studio. When I debug the project it shows no error. But when I run the project it shows following error.

 

A fatal error or exception has occurred.

  Description:   An instruction CPLB miss has occurred without a corresponding CPLB entry.

  General Type:  RunTimeError

  Specific Type: ICPLBMissWithoutReplacement

  General Code:  0x8

  Specific Code: 0x321

  Error Value:   0x00000000

  Error PC:      0x00000000

 

I went through many threads on this topic in engineer zone. But I couldn't get an ultimate solution. I am a UG student. I need an answer which I can understand with less difficulty.

Thank You in advance.

Outcomes