AnsweredAssumed Answered

Maximizing efficiency at 5 mA while using ADuM3070

Question asked by Ivan-Rusov Employee on Oct 23, 2014
Latest reply on Oct 27, 2014 by Ivan-Rusov

Hi,

 

ADuM3070 datasheet contains following efficiency graph:

I plan to use 5V input voltage and 3.7V output voltage with 5mA maximum (1.5mA typical) load current. I would like to create effective isolated power supply for light loads (1-5 mA). Could you please recommend me right transformer or isolated solution for achieving maximum efficiency at small loads (3.7 V, 1-5 mA)?

 

Regards,

Ivan

Outcomes