AnsweredAssumed Answered

Does the AD9625-2.0EBZ work with the Xilinx evaluation board VC707?

Question asked by Chris_Aed on Oct 20, 2014
Latest reply on Oct 23, 2014 by IanB

Dear community,

 

After having some bad luck with the newest AD9625 evaluation board AD-FMCADC2-EBZ FMC (the two we tried were most probably D.O.A), AVNET recommended to us to use the somewhat older AD9625-2.0EBZ. This evaluation board is meant to be used in combo with the corresponding AD data grabber board (featuring a Virtex-6 FPGA with VADJ = 2.5V).

 

However, we need to process received data in real time, thus we would prefer to use the board in combo with a VC707 featuring a Virtex-7 FPGA with VADJ = 1.8V. The pinning of the FMC connector seems to be fine but we are wondering if the the lower VADJ of the Virtex-7 (1.8V) might pose a problem?

 

Best regards

 

Chris

Outcomes