AnsweredAssumed Answered

Query related to RF trnasceiver design

Question asked by Hao on Oct 7, 2010
Latest reply on Oct 12, 2010 by enash
I want to design RF trascevier System with following features:
1. Frequency Range : 2.4GHz to 2.4835GHz
2. Transmiter Power : 30dBm
3. Receiver Sensitivity : -104dBm at 2.4Mbps
So, Please suggest any IC or ICs which can full fill above requirments.
I had a look of IC AD7242, but its output power is upto 5dBm and I require upto 30dBm. If you can suggest me any additional IC or a reference circuit by which I can increase the transmit power up to 30dBm, then it will be a great help for me.
Thanks!

Outcomes