AnsweredAssumed Answered

ADV7619 DATA_BLANK_EN

Question asked by rpmarchand Employee on Oct 17, 2014
Latest reply on Oct 20, 2014 by GuenterL

Hello,

 

in the ADV7619 HW manual there is a bit called DATA_BLANK_EN which is not referenced anywhere else in the document.  As well there is a bit called AV_BLANK_EN on figures 44 and 45.  are these bits the same?

 

Also if i clear the bit DATA_BLANK_EN does the audio information show up on the pixel bus or is the audio information only available on the audio bus?

 

Thanks

Outcomes