AnsweredAssumed Answered

Selection help for 2GHz, +26dB gain, differential amplifier

Question asked by Kevin.G Employee on Oct 10, 2014
Latest reply on Oct 12, 2014 by kkaya

I have a 2GHz, single-ended, +0dBm signal that I need to amplify and turn into two +20dBm signals that are 180 degrees out of phase with each other.  Basically a single-ended to differential amplifier with a gain of +26dB would do what I want if I could find such a chip.  Do you have anything that will work?  It doesn't have to be a single-chip solution.  If two or more chips could accomplish the same thing that would be fine.

Outcomes