AnsweredAssumed Answered

AD-FMCMOTCON1-EBZ Reference Design .tcl doesn't build in Vivado 2014.2

Question asked by nick.wernicke@gmail.com on Oct 9, 2014
Latest reply on Oct 13, 2014 by AdrianC

I have a AD-FMCMOTCON1-EBZ motor control kit for a Zedboard. I am not able to build the Vivado reference design for the programmable logic as detailed here: http://wiki.analog.com/resources/eval/user-guides/ad-fmcmotcon1-ebz/reference_hdl/linux

 

Supposedly you clone the github repo:

https://github.com/analogdevicesinc/hdl/tree/master/projects/motor_control

 

Then open Vivado and in the tcl console type:

cd [project_path]/projects/motor_control/zed

source ./system_project.tcl

 

It starts making a project but won't finish. This is the error:

 

ERROR: [BD 5-216] VLNV <xilinx.com:ip:processing_system7:5.3> is not supported for this version of the

 

 

tools.The latest version is:5.4

ERROR: [Common 17-39] 'create_bd_cell' failed due to earlier errors.

 

 

    while executing

"create_bd_cell -type ip -vlnv xilinx.com:ip:processing_system7:5.3 sys_ps7"

    invoked from within

"set sys_ps7  [create_bd_cell -type ip -vlnv xilinx.com:ip:processing_system7:5.3 sys_ps7]"

    (file "../../../projects/common/zed/zed_system_bd.tcl" line 46)

 

 

    while executing

"source $ad_hdl_dir/projects/common/zed/zed_system_bd.tcl"

    (file "system_bd.tcl" line 3)

 

 

    while executing

"source system_bd.tcl"

    (procedure "adi_project_create" line 94)

    invoked from within

"adi_project_create motor_control_zed"

    (file "./system_project.tcl" line 5)

Outcomes