AnsweredAssumed Answered

How to read meters on the RMS dynamics Processor

Question asked by Brettcoupe on Oct 4, 2010
Latest reply on Mar 24, 2011 by Brettcoupe

Hi.

I am using the RMS compressor with the 2 meters (gain reduction,  and input level)

 

I want to read these 2 meters out to the microcontroller at run time.

 

Below are the parameters

 

 

Safeload Write
Time:  18:11:46 - 634ms
Cell Name:  PROC_WB_Comp
Param Name:  TwoChannelSingleDetectAlg51
Param Address:  60
Param Value:  3.61073040962219
Bytes:  136
Param Data:
0x01,  0xCE,  0x2C,  0x6A,
0x01,  0xCE,  0x2C,  0x6A,
0x02,  0x0C,  0x24,  0xF8,
0x02,  0x52,  0x6C,  0x99,
0x02,  0xA2,  0x20,  0xC9,
0x02,  0xFC,  0x84,  0xCD,
0x03,  0x63,  0x07,  0x8C,
0x03,  0xD7,  0x49,  0x2D,
0x04,  0x5B,  0x21,  0x4B,
0x04,  0xEE,  0xC0,  0xE0,
0x05,  0x84,  0xCD,  0x97,
0x06,  0x0B,  0x2E,  0x19,
0x06,  0x74,  0xCF,  0xFC,
0x06,  0xBB,  0x4A,  0xD0,
0x06,  0xE0,  0x9B,  0x13,
0x06,  0xEB,  0x54,  0x82,
0x06,  0xE5,  0xC6,  0x9B,
0x06,  0x30,  0xCB,  0x00,
0x05,  0x9E,  0x5D,  0xB8,
0x04,  0xF4,  0x3E,  0x65,
0x04,  0x43,  0xC1,  0xAD,
0x03,  0x9A,  0x06,  0xB1,
0x03,  0x00,  0x26,  0x3F,
0x02,  0x7B,  0x24,  0x69,
0x01,  0xFB,  0x7F,  0x12,
0x01,  0x99,  0x59,  0xF4,
0x01,  0x47,  0xE6,  0xAD,
0x01,  0x04,  0xF0,  0xB2,
0x00,  0xCE,  0x75,  0x30,
0x00,  0xA2,  0x99,  0x7F,
0x00,  0x7F,  0xAA,  0x1D,
0x00,  0x64,  0x1C,  0xF9,
0x00,  0x4E,  0x80,  0xAE,
0x00,  0x3D,  0x8E,  0x98


Safeload Write
Time:  18:11:46 - 634ms
Cell Name:  PROC_WB_Comp
Param Name:  TwoChannelSingleDetectAlg51RMS_disp
Param Address:  94
Param Value:  0.000479817390441895
Bytes:  4
Param Data:
0x00,  0x00,  0x0F,  0xB9


Safeload Write
Time:  18:11:46 - 634ms
Cell Name:  PROC_WB_Comp
Param Name:  TwoChannelSingleDetectAlg51RMS
Param Address:  95
Param Value:  0.000575780868530273
Bytes:  4
Param Data:
0x00,  0x00,  0x12,  0xDE


Safeload Write
Time:  18:11:46 - 634ms
Cell Name:  PROC_WB_Comp
Param Name:  TwoChannelSingleDetectAlg51post_gain
Param Address:  96
Param Value:  1
Bytes:  4
Param Data:
0x00,  0x80,  0x00,  0x00


Safeload Write
Time:  18:11:46 - 634ms
Cell Name:  PROC_WB_Comp
Param Name:  TwoChannelSingleDetectAlg51hold
Param Address:  97
Param Value:  0
Bytes:  4
Param Data:
0x00,  0x00,  0x00,  0x00


Safeload Write
Time:  18:11:46 - 634ms
Cell Name:  PROC_WB_Comp
Param Name:  TwoChannelSingleDetectAlg51decay
Param Address:  98
Param Value:  0
Bytes:  4
Param Data:
0x00,  0x00,  0x00,  0x00

 

is the

Param Name:  TwoChannelSingleDetectAlg51RMS_disp

the METER? and if So should there be 2 . One for the Input Meter and One for the Gain Reduction meter?

 

Thanks

Brett

Outcomes