AnsweredAssumed Answered

1701 how to make tone volume dependent on input level

Question asked by bruce on Oct 3, 2010
Latest reply on Oct 19, 2010 by bruce

I am using the 1701 evaluation card.  I would like to adjust the volume/level of a sine wave tone such that it would be dependent on the RMS input level of the audio.

 

For example if the RMS input level falls below -12dB and stays that way for over 60 seconds then the tone level needs to change to half it’s full volume.  When the input level goes above –12dB then the tone level needs to change to full volume.

 

Is something like this possible in Sigma Studio?

Outcomes