AnsweredAssumed Answered

ADXL375 - Data interpretation

Question asked by fabianbreite on Oct 7, 2014
Latest reply on Oct 7, 2014 by Achim

Hello,

 

I need some help by interpreting my data from the ADXL375.

 

The register 0x31 is set to 00001011.

 

For the lsb of each axis i receive values from 0 to 254 in steps of 2.

For the msb of x and y axis i receive only 0 and by z only 255.

 

Which kind of information does the msb deliver in these cases?

Does the lsb values from 0 to 255 represent the intensity from -200 up to +200? or is there a bit for the sign?

 

Best reguards,

Fabian Breite

Outcomes