AnsweredAssumed Answered

Problem Migrating Visual DSP++ to CCES

Question asked by Krishnamangegowda on Oct 3, 2014
Latest reply on Oct 3, 2014 by CraigG

Hi,

I am using the custom target board SHARC ADSP 21489. I am trying to migrate the project that works fine in Visual DSP++ to CCES.

I have tried with default LDF file with some modification in the memory section. It seems to compile, Link and able to generate the .dxe file. I can load the .dxe file to the target and it jumps to main after the initialization. Then if I run the project it throws following fatal error.

 

A fatal error or exception has occurred.

  Description:   No dispatched handler available for the specified interrupt code.

  General Type:  RunTimeError

  Specific Type: NoDispatchedHandler

  General Code:  0x8

  Specific Code: 0xb

  Error Value:   0x02001010

  Error PC:      0x001243fe

 

Have anyone have faced this problem. Please reply as soon as possible. It's kind of urgent.

 

Thanks,

Krishna.

Outcomes