AnsweredAssumed Answered

ADV7441A DVI with 2 Links

Question asked by JimNJ on Oct 1, 2010
Latest reply on Oct 1, 2010 by DaveD

Nevermind. I see that the 2 DVI are separate, selectable video inputs and not 2 DVI links for one video input..

 

Using the ADV7441A,  I have a requirement for using both DVI links (pixel rate >165MHz.) I want to convert the video to YCrCb so it looks like Mode 6 is what I need running in DDR. I only see timing diagrames for SDR. With 2 DVI links running DDR on which edge of LLC will be the even and which the odd pixels. On what edge of LLC does DE change?

Outcomes