AnsweredAssumed Answered

Problem about the differential outputs of ADRF6510

Question asked by lilimo on Oct 1, 2014
Latest reply on Oct 8, 2014 by lilimo

Hi,

 

I used demodulator ADL5380 to convert my measured signals to DC by removing the baluns on its evaluation board. And then I connected ADL5380 with ADRF6510 evaluation board (I also removed the baluns at the input and output port) to filter and amplify I/Q signals. If I would like to connect the differential output of ADRF6510 to an oscilloscope, how can I do? In CN-0248, the differential outputs from ADRF6510 are connected to AD8130-EBZ to convert differential signals to single-ended. Are there any AD components instead of AD8130-EBZ which can interface ADRF 6510 evaluation board with the oscilloscope? Does only this AD8130 perform this function?

 

Can I directly use ADC-based Data Acquisition (DAQ) device to connect to the differential outputs of ADRF6510?

 

I am appreciating your help!

Outcomes