AnsweredAssumed Answered

ADCMP572 CML levels

Question asked by meir.mardechayev@phnx.co.il on Oct 1, 2014
Latest reply on Oct 29, 2014 by Stephen_Nugent

Hello,

 

Accubeat, one of customers are using the comperator ADCMP572 with CML differential output.

The output of the ADCMP572 is connected to the input of the MUX of ON SEMICONDUCTOR - NB6L56 - attached data sheet.

The input levels of the NB6L56 are: Vin(H)min=1.2V; Vin(L)max=1.1V

These levels are not meet the output levels of ADCMP572.

 

How can I connect between them and coordinate the output levels of  ADCMP572 and inputs of NB6L56

 

Thanks

Meir

Attachments

Outcomes