AnsweredAssumed Answered

AD5621 Offset Voltage

Question asked by Robert1980 on Sep 29, 2014
Latest reply on Oct 9, 2014 by Robert1980

The datasheet of the AD5621 states the following offset error range:
typical value +/- 0.063 mV
maximum +/- 10 mV

As this is a very broad range I'd like to know under what conditions we have to
expect the maximum value.
In our application we use the DAC output as a kind of reference voltage.
+/-0.5mV offset would be acceptable.

The ambient temperature range is between 0°C and 60°C.


Who has experience with the AD5621 and can help on that topic?


Regards

Robert


Outcomes