AnsweredAssumed Answered

Critical Warnings when building library axi_ad9122, zc702 + FMCOMMS3 Ref Design

Question asked by nick_iliev on Sep 25, 2014
Latest reply on Sep 25, 2014 by CsomI

I have an issue when building the reference  HDL design for the  ZC702+FMCOMMS3 boards  that I downloaded from GitHub.

I'm following the instructions from the  ADI Reference Designs HDL User Guide :

 

http://wiki.analog.com/resources/fpga/docs/hdl  

 

Following the "Building on VIVADO "  section,    I've installed Xilinx  Vivado 2013.4 

 

and issued the instructions listed in  " Building on VIVDAO - Library " :

 

cd c:/github/hdl/library/axi_ad9122

source ./axi_ad9122_ip.tcl

 

the above tcl script generated the following  CRITICAL WARNINGS :

 

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_mul.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_dds_sine.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/up_xfer_cntrl.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_dds_1.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/up_xfer_status.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/up_drp_cntrl.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/up_dac_channel.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/up_clock_mon.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_rst.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_mmcm_drp.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_dds.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/up_dac_common.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_serdes_out.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_serdes_clk.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/up_axi.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_mul.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_dds_sine.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/up_xfer_cntrl.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_dds_1.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/up_xfer_status.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/up_drp_cntrl.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/up_dac_channel.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/up_clock_mon.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_rst.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_mmcm_drp.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_dds.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/up_dac_common.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_serdes_out.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/ad_serdes_clk.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/github/hdl/library/common/up_axi.v' appears to be outside of the project area c:/github/hdl/library/axi_ad9122.

 

 

a few INFO: messages follow these WARNINGs , and  then it ends with :

 

 

1

update_compile_order -fileset sim_1

 

Do I have to fix these CRITICAL WARNINGs in order to compile a valid  axi_ad9122 library component ?

If so, how do I fix them  ?

Outcomes