AnsweredAssumed Answered

AD-FMCOMMS2-EBZ  linux target scripts

Question asked by Nick-AD on Sep 25, 2014
Latest reply on Oct 6, 2014 by larsc
Branched to a new discussion

Hello to all,

I compiled petalinux kernel correctly  (I hope so...) for AD-FMCOMMS2-EBZ and ZEDBOARD.

 

The board  boostraps correctly and i can login in Petalinux as root.

 

I have download the script files git from here https://github.com/analogdevicesinc/fmcomms2-scripts.git

and i follow this tutorial page Shell Scripts for the FMComms2 Board [Analog Devices Wiki]

 

after boot, i wrote this command   'dmesg | grep ad9361'

 

this is the output from console

 

root@zynq:/# dmesg | grep ad9361

platform 79020000.cf-ad9361-lpc: Driver cf_axi_adc requests probe deferral

ad9361 spi32766.0: ad9361_probe : enter

ad9361 spi32766.0: ad9361_probe : AD9361 Rev 2 successfully initialized

cf_axi_dds 79024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (4.00.b) at 0x79024000 mapped to 0xe0838000, probed DDS AD9361

ad9361 spi32766.0: ad9361_dig_tune: Tuning RX FAILED!

ad9361 spi32766.0: ad9361_dig_tune: Tuning TX FAILED!

cf_axi_adc 79020000.cf-ad9361-lpc: ADI AIM (4.00.b) at 0x79020000 mapped to 0xe0858000, probed ADC AD9361 as MASTER

 

I run the script 'fmc2_dds_buf_random.sh'

 

the output says that it can't find the device under /dev

 

what's wrong???

 

Thanks

 

Nicolas

Outcomes