AnsweredAssumed Answered

The ADV7619 with the input source of 4K*2K

Question asked by jackysj.wang@arrowasia.com on Sep 23, 2014
Latest reply on Sep 24, 2014 by jackysj.wang@arrowasia.com

Dear

      I want to make a solution of the source of HDMI 4K*2K, with the output is RGB mode. Use two ADV7619, the solution can be OK?

If OK, the Clock need to be divided, what  performence dose the Jitter be limited to ??

Outcomes