AnsweredAssumed Answered

ADV7619 4k detection and output pinout

Question asked by Nbenpaz on Sep 23, 2014
Latest reply on Sep 28, 2014 by Nbenpaz

Hello ADI experts

I'm at the beginning of design a product based on the ADV7619 and have some question.

1. Does the chip recognize the resolution of 4k as the other resolutions , in a different way or can't do it at all?

2. Is there is any output port combination that can have same pixel configuration for HD resolutions and the UHD resolution?

I did not see any way to connect the output bus to a video processor that can have the same pins connected rather using a FPGA to mux the pins in the way.

 

Naftali

Outcomes