AnsweredAssumed Answered

ADV8005 OSD Function-We need Technical support

Question asked by echo.wang on Sep 18, 2014
Latest reply on Sep 25, 2014 by mattp


I am using ADV8005 to develop 4K test instrument now, We meet below two issues:

1. Did ADV8005 could support OSD full screen display?

We want use this function to display some special picture.

2.If there are no signal input, Could ADV8005 adjust the OSD resolution to 720P or more lower?

If the signal input is 720P, But ADV8005 resolution is 1080P, It will be unrecognized.

 

ADV8005 is very new project, Please kindly extend you help, Thanks.

Outcomes