AnsweredAssumed Answered

is possible that parallel multi ADP5090 SYS pin to increase the power

Question asked by kj.liu on Sep 17, 2014
Latest reply on Sep 18, 2014 by Kevin.Yao

Hi Sir,

One of my customer is interested in ADP5090 performance but the question is their max solar power is around 1W and ADP5090 is only around 300mW, so the customer asked me that is it possible that parallel multi  ADP5090 to increase the power?  if yes, they can make the number of solar panels divide into half and half and then, they could use two ADP5090 to achieve their goal.

Outcomes