AnsweredAssumed Answered

ADV7341 Composite Output issue

Question asked by preetin on Sep 12, 2014
Latest reply on Sep 23, 2014 by PaulS

Hi,

 

We are using ADV7341 Chip for Composite output ( PAL Output) .We are observing video output with 30 pixel clipped at left and right side. The configuration is as below.

 

  i2c_write(base, reg>>1, 0x00, 0xFC ); //All DACs enabled. PLL enabled

  i2c_write(base, reg>>1, 0x01, 0x00 ); // SD input mode

  i2c_write(base, reg>>1, 0x80, 0x05 ); // PAL & NTSC standard. SSAF luma filter enabled. 1.3 MHz chroma filter enabled

  i2c_write(base, reg>>1, 0x82, 0xc4 ); //Pixel data valid

  i2c_write(base, reg>>1, 0x87, 0x20 ); //PAL/NTSC autodetect mode enabled

  i2c_write(base, reg>>1, 0x88, 0x00 ); // 8-bit input enabled

 

Please check and let me know if any problem is there in configuration.

 

Thanks & Regards

Preeti

Outcomes