AnsweredAssumed Answered

ADSP-21489BSWZ-4B: Automotive Grade and MediaLB  capability

Question asked by @kerwin on Sep 12, 2014
Latest reply on Sep 15, 2014 by @kerwin

I want to maximize the capabilities of the  ADSP-21489BSWZ-4B but Im confused with 2 issues:

1. Is it automotive grade?

          the highest temperature stated from the datasheet is 85 degrees Celsius wherein it should be 125 degrees Celsius as any           standard category of IC in semiconductor, automotive application.

          I want to clear this issue due to the application of my project

 

2. Is ADSP-21489BSWZ-4B capable with MediaLB?

          the datasheet states the series ADSP21489 has a MediaLB while referring to the evaluation board it contradicts the datasheet

 

any ADI FAE comments, suggestions is highly appreciated.

Outcomes