AnsweredAssumed Answered

ADRF6510 software not working

Question asked by biancajs on Sep 9, 2014
Latest reply on Jul 28, 2015 by jdobler

I have recently started using the ADRF6510 evaluation board. I have installed the software but when I use it to write a cutoff frequency to the device the frequency read back is always "1", regardless of what I try to write. Using an oscilloscope probe to measure the signal being sent to the board when I write to it, it seems that it consists of two pulses, the first changes depending on what frequency I set, and the second is always the same - so maybe this second pulse is setting it back to 1?

 

I've tried this on both a Vista machine and a Win7 (with drivers I found in another post on here) and the same thing is happening on both.

 

Any suggestions would be appreciated,

 

Thanks,

Bianca

Outcomes