AnsweredAssumed Answered

EVAL-ADAU170XEBZ trouble writing to EEPROM

Question asked by audiolab1 on Sep 23, 2010
Latest reply on Jun 14, 2011 by BrettG

I've just started evaluating the ADAU1701 eval board and I am not able to write my compiled project to the on-board EEPROM. The code runs fine as confirmed by my Audio Precision, but the code is not loading to the EEPROM. I right click on the 1701 in the Hardware Configuration tab and select "Write latest complied to E2PROM". It goes through the write process but then when I reset the board there is no code loaded and no signal is passed. I'm pretty sure I have the switches and jumpers set correctly but the documentation is very vague in this area. Going under the read/write tab for the EEPROM and pressing "Download file to E2PROM" gives me an unhandled exception error and again nothing is loaded to the EEPROM. Any suggestions would be appreciated!

Outcomes