AnsweredAssumed Answered

ADV7181C / ADV7403

Question asked by ofirvaknin on Sep 3, 2014
Latest reply on Sep 9, 2014 by DaveD

Hi

I have few questions regarding ADV7181C, ADV7403 and similar products

 

1. Is there any way to use the ADV7181C for SXGA resolution. (I prefer using this device because it is small package device)

2. According to the data sheetThe ADV7403-140  can be used for SXGA but it is not industrial. Is it possible to use the industrial device ADV7403-110 to resolution of SXGA (SXGA pixel clock is 108Mhz which is below 110Mhz)

3. Do the devices supports 50Hz XGA / SXGA ?

 

Thanks alot

 

Ofir

Outcomes