AnsweredAssumed Answered

ADL5385 evaluation board for IQ modulation

Question asked by reduction on Sep 3, 2014
Latest reply on Oct 12, 2014 by THA

Hello all,

I would like to use ADL 5385 evaluation board for amplitude, phase and frequency modulation of RF signal. The center frequency is 300MHz.

1. Does DC signal work as I and Q input? If so, different voltage level of I and Q inputs modulate the phase. (Sorry for this simple question. Our oscilloscope is not working so I cannot check it)

2. For frequency modulation, I observe poor suppression for higher order sidebands as shown in the figure. The parameters follow the manual, with 0.7V for I and Q differential input with a 0.5V DC bias; 600MHz LO at -7dBm. Then I fine tune Vp-p and phase for the I and Q signal respectively to better suppress the sidebands (0.001V and 0.1degree resolution). Generally, the baseband feedthrough and the first sideband is suppressed okay. But we get only ~20dB suppression for higher order sidebands. For comparison, the result without DC bias is attached.


Our goal is to get at least 30dB suppression from this. Any suggestions?

Thanks!

Attachments

Outcomes