AnsweredAssumed Answered

ADV7511 Set resolution question

Question asked by bkl on Sep 3, 2014
Latest reply on Sep 5, 2014 by larsc

I download the reference design on the zedboard and also build the kernel to make the board working correctly(I removed the SPI device, only the video output). But now, I want to change some function about the adv7511.

1、No matter if the HDMI device connect to the board, the resolution is set to 1366*768.

2、No matter if the HDMI device connect to the board, the VDMA always transfer the frame_buffer data(1366*768)

 

So, How could I modify the driver in the kenel source. Thank you for your help!

Outcomes