AnsweredAssumed Answered

PGO error

Question asked by wallman16 on Sep 1, 2014
Latest reply on Sep 24, 2014 by Suraj

Hi ,

 

I have a problem with PGO on BF70x .

I have enabled PGO and i get .PGO file after run . But encounter error .

 

Code is simple :

No Hardware need BF533 VDSP++ example

#include "adi_initialize.h"

#include "FFT.h"

#include <fract.h>

#include <filter.h>

 

#define VEC_SIZE 256 // length of the input vector

#define NUM_TAPS 8 // number of filter coefficients

 

fract16 in[VEC_SIZE] = {

#include "in.dat"

};

 

 

fract16 coefs[NUM_TAPS] = {

#include "coefs.dat"

};

 

fract16 delay[NUM_TAPS];

 

fract16 out[VEC_SIZE + NUM_TAPS - 1];

 

fir_state_fr16 state; // declare filter state

int main(void)

{

  /**

  * Initialize managed drivers and/or services that have been added to

  * the project.

  * @return zero on success

  */

  adi_initComponents();

 

  fir_init(state, coefs, delay, NUM_TAPS, 1); // initialize filter state

  fir_fr16(in, out, VEC_SIZE, &state); // apply the filter to the data

 

}

 

error.jpg

Outcomes