AnsweredAssumed Answered

ADV3003 - Is there a min Voltage spec on VTTO & VTTI

Question asked by Tim@TLendeavors on Sep 20, 2010
Latest reply on Sep 8, 2011 by daverowe

I am trying to interface TMDS to 1.2V ASIC.  So the architecture would be TMDS -> ADV3003 -> ASIC -> ADV3003 -> TMDS.  Can I hook the VTTI and the VTTO that interface to the ASIC to 1.2V (or lower)?  Will this limit the max output votage to 1.2V??

 

The data sheet only specs a MAX value and gives the following very vague comment:

The supplies can also be powered individually, but care must be taken to ensure that each stage of the ADV3003 is powered correctly.

 

 

Thanks

Tim

Outcomes