AnsweredAssumed Answered

Using the ADP2384 on a test board

Question asked by agrimes Employee on Aug 28, 2014
Latest reply on Aug 28, 2014 by power-layout-guy

I am designing a Final Test board and am planning on using the ADP2384 to provide the 2.5V supply for two ADN4612 matrix switch devices. I have used the ADIsimPower tool to design the regulator circuit but would like it reviewed by an Apps engineer to verify that it will work as expected before I proceed to manufacture of the pcb. Each ADN4612 could draw a maximum current of 1.5A . My main concern would be possible ripple in the output voltage of the regulator affecting the follow on circuitry.

Outcomes