AnsweredAssumed Answered

ADN4600 Register Operation

Question asked by BabyBabyQ on Aug 28, 2014
Latest reply on Sep 3, 2014 by jmarshma

Hi:

 

I'm using ADN4600 and I have some questions about how to connect the inputs to the outputs by operating the registers.

1. How to realize the connectivity between the inputs and the outputs? For example,I want to connect Input[0] to Output[0],Input[1] to Output[1],Input[2] to Output[2] and so on, do I need to write register 0x41 every time after I have writed register 0x40?Or,I just need to write register 0x41 only once after I have programmed all outputs?

 

2. Does it change the previous connections by writing register 0x41? For example, at the first time, I connect Input[0] to Output[0],Input[1] to Output[1],Input[2] to Output[2], then update(by writing register 0x41). After that, I connect Input[0] to output[3] but don't operate other outputs,then I update.After this operation, do the other two connections still exist? And does the connection of Input[0] to Output[0] still exist?

 

I'm looking forward to any valuable recommendations and suggestions.

Outcomes