AnsweredAssumed Answered

Boot up from flash with DSP 21368, difference between released or debug built code?

Question asked by zooho on Sep 20, 2010
Latest reply on Sep 23, 2010 by CraigG

Hi, there

 

I have a question with the booting up from flash issue:

 

We have dual DSP 21368 in one board and it could boot up from debug version code but has some problem with released version code. Can you tell me what's the difference between the debug built and release built?

 

I tried to disable the " Optimization" in release version, the same result.

 

I am not sure what else I should look at? Any registers setting or else? They are using the same kernal file for loader, same code...

 

 

Thanks for any suggestion.

 

Tao Zhao

Outcomes