AnsweredAssumed Answered

Linker/Locator 256K of Code

Question asked by tcmichals on Aug 27, 2014
Latest reply on Aug 29, 2014 by CraigG

Looking at using BF70x part and want to know if it is possible to use the linker/locator to load code into L2 SRAM?   For example, use only 256K of L2 SRAM and still use a Quad-SPI execute in place for non-critical code.  Is there special startup code that copies the code into L2 SRAM? (The ROM used sections in the dxe to know where to copy code, does this still exist?)

 

Is there a tool to assist placing which module of code into L2 SRAM?

Outcomes