AnsweredAssumed Answered

Sigma Studio Ver 3.11 Build 1. Rev 1356 Mixer Bug?

Question asked by mharkins on Aug 21, 2014
Latest reply on Oct 21, 2014 by mharkins

 

I'm running Sigma Studio Ver 3.11 BUild 1. Rev 1356.  And I have a 4 input, 3 output mixer.  My assumption from reading the literature is that the inputs are represented by the rows of controls, while the outputs are the columns creating a 4-row, 3-column mixer board.  My issue is that when I set up the first row (input) for the desired outputs, and set the remaining three rows (9 controls) to -200dB, I still get bleed through from the inputs that are effectively turned off.  I proved this by inserting mute blocks into the input lines and muting them and my bleed through signal disappeared.  Is there an issue with this control, or am I misunderstanding something?

 

 

 

Outcomes