AnsweredAssumed Answered

AD9880 IBIS model with drive strengths

Question asked by JamesL on Sep 17, 2010
Latest reply on Oct 18, 2010 by cvaughn

Hi

 

I'm trying to simulate the AD9880 pixel output interface in my design.

I have the IBIS model for the AD9880 dated 16/9/2004, Rev 0.

It seems to work fine, but it only has one model type assigned to the CLK and DATA pins, whereas the datasheet for the part describes at least two drive strengths as per register 0x25 bits 5:4.

 

Is there a more recent IBIS model with both drive options and if not, which drive strength does this model in this IBIS file correspond to?

 

Thanks

James.

Outcomes