AnsweredAssumed Answered

FMCOMMS1-ebz - Bandwidth tech spec. clarification

Question asked by omkarpradhan on Aug 19, 2014
Latest reply on Aug 26, 2014 by charlyelkhoury

1) I'd appreciate a clarification on the tech specs for this device.

 

 

The clarification requested is with respect to: 125 MHz channel bandwidth

 

 

Can I please know which one is it?

 

2) In this case then does this mean that between 400 Mhz and 4 GHz one can tune this transceiver at any center frequency with 125/200 MHz bandwidth?

 

3) I'm guessing the channel bandwidth is a figure associated with the analog receiver portion of this module, right?

 

4) My application has a 0.75-1 GHz Antenna as the Rx/Tx, FMCW sweep over this 250 MHz bandwidth. So am I right in concluding that this product is then NOT appropriate for my application? Am I reading this right?

Outcomes