AnsweredAssumed Answered

Tx performance at high freq

Question asked by aries on Aug 13, 2014
Latest reply on Aug 14, 2014 by aries

Using 9361 at 3.6 GHz.

The datasheet lists max power at +7 dbm. Uncertain if Linear or Psat. See mask plots as function of gain, but found only at 800 MHz.

On our board or ADI Eval board, (single-tone) can observe up to +2 dBi and already saturated.

Any more info on the Tx performance above 3 GHz ?

Using a 50 Ohms narrow-band Balun. With a small cap between the diff ports can gain another 1-2 dbm.

Outcomes