AnsweredAssumed Answered

ADV7619 VSYNC output issue

Question asked by arpad.maroti@lightware.eu on Aug 13, 2014
Latest reply on Sep 11, 2014 by PaulS

Hi,

 

I am using an ADV7619 to receive 4k HDMI signal. It's pixel bus is configured in 2x24-bit 4:4:4 SDR interleaved mode. The pixel bus is connected to an FPGA.

 

I have an issue, that sometimes, when I switch video on the input, the ADV7619 is not able to produce correct VSYNC signal. At vs_bad1.png, the signal changes it's value 4 times within a single frame.

However, sometimes it works perfectly fine. The correct VSYNC should look like the one on vs_good.png.

 

By switching the input HDMI on and off, i was able to produce the two images with the same configuration.

 

Sometimes, I've experienced small glitches in the signal too (see vs_bad2.png).

 

Can you give me some advice please? I think the problem may be at the HDMI input side, but I'm not sure. In both cases, I was able to read out correct frame measurements from the ADV7619.

 

Thanks,

Arpad Maroti

Attachments

Outcomes