AnsweredAssumed Answered

question: visual audio program boot from 21369EZ-LITE?

Question asked by lenjohn on Sep 13, 2010
Latest reply on Sep 28, 2010 by DeepV

I am using Visual Audio 2.6 designed one simple program using 21369EZ-LITE,and generated code ,then turn to VDSP5++,i can build the project (project->options ->type is "executable file") and connect the EZ-LITE,and working well, then i select project->options, and select type->"loader file",and then i bulid the project and generate the .ldf file, then i use tools->program,write AMDflash ,the program flash progress is well ,without any question, but when i restart the board, the program can't work. who can tell me what i need to do?or i miss something?

Outcomes