AnsweredAssumed Answered

BF592 Ezkit Won't Connect to PC

Question asked by Taylord on Aug 11, 2014
Latest reply on Aug 12, 2014 by Taylord

Hi all,

 

I have the BF592 Ezkit Lite, and it seems to have troubles connecting to Crosscore or windows in general. When I try to begin debugging in Crosscore there are three errors messages that are shown. The first two are java.lang.nullpointerexception and the third is as follows:

 

Error in launch sequence

[TpsdkServer] Failed to connect to processor.

 

Error: 0x80048020

Error Description: Selected emulator not detected

 

This may not be relevant as I don't believe the device connects to windows 7 at all. I say this because it will not show up in device manager. On the rare chance the device does show up in device manager then it will work fine in Crosscore. There are 2 specific LEDs that light up when it does decide to connect, but I can't find any way to get the board into this state other than to keep trying until it finally works (rarely).

 

If anyone knows of a solution or has had a similar problem I would greatly appreciate your help. Thanks,

 

Taylor

Outcomes